Hello,
I see there are pad mux in u-boot board file, and also in kernel device tree files.
Both seems to be about the same.
So, Why is it that both are required ? Why can't u-boot pad also keep on when moving to kernel ?
I am afraid that there might be some differences between both.
Is it that CONFIG_PINMUX shall disable the override of mux in kernel ?
Thank you,
Ran
解決済! 解決策の投稿を見る。
Hi Ran
u-boot pad configs can keep on when moving to kernel using dts settings
described in linux/Documentation/devicetree/bindings/pinctrl/fsl,imx-pinctrl.txt:
Bits used for CONFIG:
NO_PAD_CTL(1 << 31): indicate this pin does not need config.
linux-imx.git - i.MX Linux Kernel
Since uboot and kernel may be used with other os&bootladers, so seems both pad mux
are used.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ran
u-boot pad configs can keep on when moving to kernel using dts settings
described in linux/Documentation/devicetree/bindings/pinctrl/fsl,imx-pinctrl.txt:
Bits used for CONFIG:
NO_PAD_CTL(1 << 31): indicate this pin does not need config.
linux-imx.git - i.MX Linux Kernel
Since uboot and kernel may be used with other os&bootladers, so seems both pad mux
are used.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------