P1010/14 single bit ECC NAND

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

P1010/14 single bit ECC NAND

跳至解决方案
2,084 次查看
renaud
Contributor IV

We are using a P1014 with a SLC NAND using 1-bit ECC. Hence, we do not use the hardware ECC support.

The Linux (v 3.14.0) driver  uses the random input command which is not supported in

the FSL IFC NAND driver.  This leads to an enormous amount of messages and ECC errors reported when using the

ubiformat command. I do not see any support for that command in newer version of Linux

Is there any information that could help me implement the command?

Looking at the other drivers for idea lead me to a silent ubiformat command but did not solve the issue with

ECC errors.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,929 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,930 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
1,929 次查看
ufedor
NXP Employee
NXP Employee

Please open a Service Request to investigate the issue in more detail.

0 项奖励
回复
1,929 次查看
renaud
Contributor IV

A SR has been opened. I eventually implemented code to support the random data output command.

MTD testing (speedtest, torture, subpage) passed.  The system now boot from NAND.

Thanks to Freescale technical  support.

0 项奖励
回复
1,929 次查看
ufedor
NXP Employee
NXP Employee

Hello,

You wrote:

> We are using a P1014 with a SLC NAND using 1-bit ECC.

> Hence, we do not use the hardware ECC support.

Please clarify how ECC is calculated in your case.

0 项奖励
回复