Overrun error occurs at UART of i.MX8MQ custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Overrun error occurs at UART of i.MX8MQ custom board

Jump to solution
5,180 Views
KentarouFujita
Contributor II

Up to 16 custom boards equipped with i.MX8MQ are connected for RS-485 communication.
We have modified the driver to support the custom baud rate and have successfully communicated at 250000bps.

However, in rare cases, the UART suffers from an overrun error and does not recover.
When this happens, it will not be able to receive at all, but it seems to be able to transmit.

Can anyone tell me what causes the overrun error to occur, or how to recover from it other than rebooting the system when it occurs?

 

BSP Ver:Linux 5.10.35_2.0.0
imx8mq-evk.dts

 

 

/* RS-485 */
&uart3 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_uart3>;
	assigned-clocks = <&clk IMX8MQ_CLK_UART3>;
	assigned-clock-parents = <&clk IMX8MQ_CLK_25M>;
	uart-has-rtscts;
	rts-gpios = <&gpio5 8 GPIO_ACTIVE_HIGH>;
	linux,rs485-enabled-at-boot-time;
	status = "okay";
};

 

Labels (2)
0 Kudos
Reply
1 Solution
5,122 Views
KentarouFujita
Contributor II
This case was due to memory corruption caused by an inadequate DRAM configuration. The problem has now been resolved. This ticket has served its purpose and is closed.

View solution in original post

0 Kudos
Reply
2 Replies
5,123 Views
KentarouFujita
Contributor II
This case was due to memory corruption caused by an inadequate DRAM configuration. The problem has now been resolved. This ticket has served its purpose and is closed.
0 Kudos
Reply
5,128 Views
Juan-Rodarte
NXP Employee
NXP Employee

Hi Kentarou,

You can upgrade to a newer BSP.

Regards

0 Kudos
Reply