Overrun error occurs at UART of i.MX8MQ custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Overrun error occurs at UART of i.MX8MQ custom board

ソリューションへジャンプ
2,489件の閲覧回数
KentarouFujita
Contributor II

Up to 16 custom boards equipped with i.MX8MQ are connected for RS-485 communication.
We have modified the driver to support the custom baud rate and have successfully communicated at 250000bps.

However, in rare cases, the UART suffers from an overrun error and does not recover.
When this happens, it will not be able to receive at all, but it seems to be able to transmit.

Can anyone tell me what causes the overrun error to occur, or how to recover from it other than rebooting the system when it occurs?

 

BSP Ver:Linux 5.10.35_2.0.0
imx8mq-evk.dts

 

 

/* RS-485 */
&uart3 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_uart3>;
	assigned-clocks = <&clk IMX8MQ_CLK_UART3>;
	assigned-clock-parents = <&clk IMX8MQ_CLK_25M>;
	uart-has-rtscts;
	rts-gpios = <&gpio5 8 GPIO_ACTIVE_HIGH>;
	linux,rs485-enabled-at-boot-time;
	status = "okay";
};

 

ラベル(2)
0 件の賞賛
返信
1 解決策
2,431件の閲覧回数
KentarouFujita
Contributor II
This case was due to memory corruption caused by an inadequate DRAM configuration. The problem has now been resolved. This ticket has served its purpose and is closed.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,432件の閲覧回数
KentarouFujita
Contributor II
This case was due to memory corruption caused by an inadequate DRAM configuration. The problem has now been resolved. This ticket has served its purpose and is closed.
0 件の賞賛
返信
2,437件の閲覧回数
Juan-Rodarte
NXP Employee
NXP Employee

Hi Kentarou,

You can upgrade to a newer BSP.

Regards

0 件の賞賛
返信