Override parts of BOOT_CFG1 by fuse?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Override parts of BOOT_CFG1 by fuse?

748 Views
alampret
Contributor I

Hi,

is it possible to override only some parts of BOOT_CFG1 by fuse?

My problem:

BOOT_CFG1 is defined by external resistors.

BOOT_MODE is set to 10 (Internal boot)

Now I need to changed SD card speed to SDR50 or SDR104 for some tests. Is it possible to override just these 2 bits? BOOT_CFG1[2,3]?

If yes, how?

Do I have to change BOOT_MODE to 00?

Thx,

Alexander

Labels (2)
0 Kudos
3 Replies

545 Views
Yuri
NXP Employee
NXP Employee

Hello,

  such scenario, when part of BOOT_CFG bits are taken from fuses and other part - from GPIO

is not supported.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

545 Views
alampret
Contributor I

Hi Yuri,

thx for your fast answer!

So in that case I have to set BOOT_CFG1 and BOOT_CFG2 in fuse, right?

What else is needed to make it work?

Thx,

Alexander

0 Kudos

545 Views
Yuri
NXP Employee
NXP Employee

Hi, Alexander !

  it is needed to burn the BOOT_CFGx, set BOOT_MODE[1:0] = 00 (Boot From Fuses)

and burn fuse BT_FUSE_SEL = 1.

Regards,

Yuri.

0 Kudos