Overlay on camera stream in i.MX8MM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Overlay on camera stream in i.MX8MM

3,448 Views
namanthaker
Contributor IV

Hello,

I am using gstreamer pipeline on i.MX8M Mini dual core platform (OS: Yocto L5.4.24-2.1.0) to capture a 5MP@20FPS camera input and put overlay on it using below command:

 

 

gst-launch-1.0 -v v4l2src device=/dev/video0 num-buffers=100 ! video/x-raw,width=2592,height=1944 ! queue ! imxvideoconvert_g2d ! video/x-raw,width=1920,height=1080 ! textoverlay text="Device name[%STATUS] reading : %%%" valignment=top halignment=left shaded-background=true ! textoverlay text="Device %Serial Number : ..%Tag location.." valignment=bottom halignment=left shaded-background=true ! clockoverlay halignment=right valignment=top shaded-background=true time-format="%H:%M:%S %D" ! vpuenc_h264 ! h264parse ! mp4mux ! filesink location=/home/root/video.mp4

 

 

Here is the expected output on the camera stream after applying the overlay.

Expected_Overlay_output.jpg

When I use the above command, CPU utilisation increases to 120% (checked with top command) and the video is recorded at 6FPS. I have debugged that the Gstreamer overlay (which is a SW element) is causing the high CPU utilisation and subsequent FPS drop.

Based on the issue I have below queries:
1. Going through the i.MX8MM datasheet and Gstreamer documents, I saw that 8MM supports overlay through GPU. If I can use the GPU to offload the SW overlay pipeline, I believe I can get full 20FPS.

Could someone suggest how I can use the GPU overlay feature to perform overlay on the input camera stream?

2. How do I confirm that the dual cores are being utilised or not? Does i.MX8MM L5.4.24-2.1.0 support any load balacing feature ? If yes, how does the load balancing between two cores work on i.MX8MM in L5.4.24-2.1.0?

3. Are there any other module/method available (preferably a HW module) to create overlay on camera stream in i.MX8MM?

Regards,
Naman

0 Kudos
Reply
5 Replies

2,717 Views
vincentz63
Contributor IV

Hi,

Thanks for the info. We ended-up using the imxcompositor in the end for our overlays, which uses nearly no CPU. Out of interest, what is the CPU usage with the Cairo library for your overlays?

0 Kudos
Reply

2,711 Views
namanthaker
Contributor IV

Hello,

The CPU utilization was around 20% with Cairo Plugin.

0 Kudos
Reply

3,408 Views
namanthaker
Contributor IV

Hello,

This issue is getting critical for us now.
Could someone please help to update on this thread.

Regards,
Naman

0 Kudos
Reply

2,922 Views
vincentz63
Contributor IV

Hello,

Did you find a way to the use the TextOverlay element on the i.MX8M Mini? Was your image built with FPU / NEON support?

Thanks

0 Kudos
Reply

2,722 Views
namanthaker
Contributor IV

Hello,

We used Cairo Overlay pluging with Gstreamer to get the overlay elements. Our image was not build with FPU/NEON support.

Cairo Overlay : https://gstreamer.freedesktop.org/documentation/cairo/index.html?gi-language=c

0 Kudos
Reply