Output SPDIFs acquired clock to a pin?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Output SPDIFs acquired clock to a pin?

244 次查看
sgordon777
Contributor I

Is there a way to output the acquired (from SPDIF-RX) sample clock to a pin, which could be used to drive other peripherals? If so can you refer me to details? We are working with I.MX8 and I.MX95 series.

Thanks

Steve

标签 (1)
0 项奖励
回复
1 回复

217 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Depending on the processor you are using, you could use CLKO pins and route the required clock this pin, here an example in the community:

Solved: enable CLKO2 for 24MHz output clock on iMX8MN - NXP Community

Best regards.

0 项奖励
回复