Output BT656 from iMX6Q to ADV7391

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Output BT656 from iMX6Q to ADV7391

Jump to solution
3,160 Views
sebastiancabot
Contributor II

Hello

I am trying to output BT656 to the ADV7391 but the output is distorted (Please see attached video)

(The pattern I am writing to the frame buffer is:

WHITE:  90 Columns

RED:    180 Columns

Green:  180 Columns

Blue:     180 Columns

Black:    90 Columns

)

We have our own board based on the Hummingboard2 from Solidrun.

I am using the latest patches for 3.14.52 from: Patch to Support BT656 and BT1120 Output For i.MX6 BSP 

The ADV7391 is connected to IPU1 DISP1 using DATA lines 0 to 7.

HDMI is connected to IPU1 DISP0

Here is the fb definition:

    mxcfb2: fb@1 {
        compatible = "fsl,mxc_sdc_fb";
        disp_dev = "adv739x";
        interface_pix_fmt = "BT656";
        mode_str = "BT656-NTSC";
        default_bpp = <16>;
        int_clk = <0>;
        late_init = <0>;
        status = "okay";
    };

    &i2c3 {
    clock-frequency = <100000>;
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_hummingboard2_i2c3>;
    status = "okay";
    adv7391: adv7391@2b {
        compatible = "adv,mxc_adv739x";
        reg = <0x2b>;
        pinctrl-names = "enable", "default";
        pinctrl-0 = <&pinctrl_i2c3_adv739x_on>;
        pinctrl-1 = <&pinctrl_i2c3_adv739x_off>;
#define GP_ADV7391_RESET <&gpio3 10 GPIO_ACTIVE_LOW>
        rst-gpios = GP_ADV7391_RESET;
        ipu_id = <0>;
        disp_id = <1>;
    };
};

Here is the pinmux definition:

pinctrl_i2c3_adv739x_on: i2c3-adv7931x-grpon {
            fsl,pins = <
                MX6QDL_PAD_EIM_A16__IPU1_DI1_DISP_CLK 0x10 /* CLOCK */
                MX6QDL_PAD_EIM_DA9__IPU1_DISP1_DATA00  0x10
                MX6QDL_PAD_EIM_DA8__IPU1_DISP1_DATA01  0x10
                MX6QDL_PAD_EIM_DA7__IPU1_DISP1_DATA02  0x10
                MX6QDL_PAD_EIM_DA6__IPU1_DISP1_DATA03  0x10
                MX6QDL_PAD_EIM_DA5__IPU1_DISP1_DATA04  0x10
                MX6QDL_PAD_EIM_DA4__IPU1_DISP1_DATA05  0x10
                MX6QDL_PAD_EIM_DA3__IPU1_DISP1_DATA06  0x10
                MX6QDL_PAD_EIM_DA2__IPU1_DISP1_DATA07  0x10
                MX6QDL_PAD_EIM_DA11__IPU1_DI1_PIN02 0x10 /* HSYNC */
                MX6QDL_PAD_EIM_DA12__IPU1_DI1_PIN03 0x10 /* VSYNC */
                MX6QDL_PAD_EIM_DA10__GPIO3_IO10 0x400130b1 /* RST */
            >;
        };

Please note that although HSYNC and VSYNC are defined they are not used since BT656 Mode is selected for the device:

Here is the device configuration for NTSC:

static void adv739x_set_ntsc(struct adv739x_data *adv739x)
{
    struct i2c_client *client = adv739x->client;
    // Reg 0x01: SD input
    adv739x_write(client, 0x01, 0x00);
    //NTSC
    // Reg 0x80: SD, NTSC
    adv739x_write(client, 0x80, 0x10);
    // Reg 0x82: SD, CVBS
    adv739x_write(client, 0x82, 0xCB);
    // Reg 0x8A: Timing mode slave use EAV/SAV
    adv739x_write(client, 0x8A, 0x08);
}

And here is the video mode definition:

static struct fb_videomode adv739x_modedb[] = {
    {
     /* NTSC Interlaced output */
     "BT656-NTSC", 60, 720, 480, 37037,
     19, 3,
     20, 3,
     276, 1,
     FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
     FB_VMODE_INTERLACED,
     FB_MODE_IS_DETAILED,},
    {
     /* PAL Interlaced output */
     "BT656-PAL", 50, 720, 576, 37037,
     22, 2,
     23, 2,
     288, 1,
     FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
     FB_VMODE_INTERLACED,
     FB_MODE_IS_DETAILED,},
};

I have changed the BT656_IF_DI_MSB in ipu_disp.c to 7

I have changed the clock definition in clk-imx6q.c to:

imx_clk_set_parent(clk[IMX6QDL_CLK_IPU1_DI1_PRE_SEL], clk[IMX6QDL_CLK_PLL3_PFD1_540M]);  /* For CVBS 27MHz clock */

Looking at dmesg I can see that the clocks are correctly configured:

[   28.061693] imx-ipuv3 2400000.ipu: pixel clk = 27000000
[   28.062233] imx-ipuv3 2400000.ipu: bt656 di clk:108000000
[   28.062260] imx-ipuv3 2400000.ipu: round pixel clk:27000000
[   28.067443] imx-ipuv3 2400000.ipu: div:4

Any help will be appreciated.

Thank you

Sebastian

Labels (3)
0 Kudos
Reply
1 Solution
2,152 Views
sebastiancabot
Contributor II

The solution for this problem was to move the HDMI to IPU1.

View solution in original post

0 Kudos
Reply
5 Replies
2,153 Views
sebastiancabot
Contributor II

The solution for this problem was to move the HDMI to IPU1.

0 Kudos
Reply
2,152 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

How about your kernel log? Is there any error?

And did you measure the clock pin frequency?

Maybe you can adjust the IOMUX, such as the "0x10":

MX6QDL_PAD_EIM_DA9__IPU1_DISP1_DATA00  0x10

0 Kudos
Reply
2,152 Views
sebastiancabot
Contributor II

Hello Qiang Li

There are no errors in the kernel log.

We measured the clock frequency using a scope and it is 27MHz.

Also as mentioned I printed the clock frquencies from ipu_init_sync_panel and the printout suggests the clock is correctly configured to 27MHz

Also the ADV7391 doesn't work if the clock is incorrect and I can use it to output the device's internal BARS pattern correctly so the clock must be correct.

I don't understand your suggestion for the iomux. right now the pins are configured with 0x10.

What would you suggest I use instead?

Thank you very much

Sebastian

0 Kudos
Reply
2,152 Views
sebastiancabot
Contributor II

Hello Igor

Thank you for your answer.

I haven't checked this on the reference board.


I don't have access to such a board and even if I did I need to make it work on our board.

Any ideas as to what I can check?

Thank you

Sebastian

0 Kudos
Reply
2,152 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sebastian

had you tried these patches on nxp reference boards with official bsp releases on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

third party boards (like hummingboard) and bsps are supported by its vendors and

one can post it on meta-fsl-arm mailing list
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply