Options available for customizing the SPL on the iMX6ULL?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Options available for customizing the SPL on the iMX6ULL?

1,824 次查看
djregan
Contributor III

Hello, Regarding secondary program loaders (SPL)...

What options are available for customizing the SPL on the iMX6ULL?

What NXP design tool suite is recommended for customizing the SPL? And, on this recommended design suite - is there a default SPL provided that can be used as the baseline for customizations?

It is through the SPL that preferrenced pin mux selections can be made on the iMX6ULL, correct? I've downloaded i.MX Pins Tool v3.0 and can create the .mex files - and, I'm ready for the next steps, whatever they are toward customizing iMX6ULL pin configuration?

Thanks much in advance...

DJ

标签 (3)
标记 (2)
0 项奖励
回复
1 回复

1,359 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi DJ,

the following links will be useful.

U-Boot Migration Example 

YOCTO uBoot: How to add support for a custom board (or OpenRex) - iMX6 Rex Projects 


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复