Oprofile not running on target

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Oprofile not running on target

ソリューションへジャンプ
2,697件の閲覧回数
bharathsambacha
Contributor I

I want to use oprofile to get profiling information for my applications on i.MX6Q sabrelite target environment.

I have selected the oprofile package in ltib and built the kernel image.

I am able booting the board using the NFS, but when I try to start the oprofile (by giving command "opcontrol --vmlinux=/home/htsl/FQuad/Build_New/Build/rootfs/boot/vmlinux")on the target I get the error message as

modprobe: module oprofile not found in modules.dep

modprobe: module oprofile not found in modules.dep

Kernel doesn't support oprofile

Also when I issue command operf it says command not found.

please help me to resolve this.

Host operating system: Ubuntu 10.04 LTS

ltib version: 9.1.1

Kernel version: 3.0.35

ラベル(2)
0 件の賞賛
返信
1 解決策
1,711件の閲覧回数
LeonardoSandova
Specialist I

Have you enabled the oprofile support on the Kernel menuconfig (it is under General Setup, Profiling Support)?

Leo

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,712件の閲覧回数
LeonardoSandova
Specialist I

Have you enabled the oprofile support on the Kernel menuconfig (it is under General Setup, Profiling Support)?

Leo

0 件の賞賛
返信
1,711件の閲覧回数
bharathsambacha
Contributor I

Hi Leo,

Thanks for the quick response, now I have enabled the kernel profiling option and oprofile support in kernel configuration and it seems to be working.

Best Regards,

Bharath S

0 件の賞賛
返信