Operating range of VDD_SNVS_IN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Operating range of VDD_SNVS_IN

Jump to solution
1,389 Views
george
Senior Contributor II

Dear All,

Please let me know about VDD_SNVS_IN for i.MX6.

Q1)

Though the operating range of VDD_SNVS_IN is specified as 2.9V - 3.3V in datasheet Table 9, there is a description of 2.8V in the SVNS only mode in Table12.

=> http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Which is the minimum value?

Q2)

When using with PMIC (MMPF0100F0AEP), in SNVS mode, Is setting change needed though the VSNVS output is 2.5V (default)?

Best Regards,

George

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,123 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

1. correct value gives datasheet Table 9 sect.4.1.3 Operating Ranges

2. MMPF0100 VSNVS output is 3.0V (default)

Table 10. Start-up Configuration

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,124 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

1. correct value gives datasheet Table 9 sect.4.1.3 Operating Ranges

2. MMPF0100 VSNVS output is 3.0V (default)

Table 10. Start-up Configuration

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,123 Views
george
Senior Contributor II

Dear Igor,

Thank you for the comment about Question 1.

And, Q2 had a typo by me.

When using with PMIC (MMPF0100F0AEP), The VSNVS output is 2.5V in OFF mode.

QSB is such at when of PowerOFF.

However, the operating range of VDD_SNVS_IN is specified as 2.9V - 3.3V in datasheet Table 9.

=> http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Is it necessary to change setting into the range?

Best Regards,

George

0 Kudos
Reply
1,123 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

one needs to have valid coincell connected to LICELL,

check MMPF0100 sect.6.4.7 VSNVS LDO/Switch

Best regards

igor

0 Kudos
Reply
1,123 Views
george
Senior Contributor II

Dear Igor,

It seems that my conditions description is not good.

I close here and I will Post it newly.

BR

George

0 Kudos
Reply