Operating range of VDD_SNVS_IN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Operating range of VDD_SNVS_IN

ソリューションへジャンプ
1,985件の閲覧回数
george
Senior Contributor II

Dear All,

Please let me know about VDD_SNVS_IN for i.MX6.

Q1)

Though the operating range of VDD_SNVS_IN is specified as 2.9V - 3.3V in datasheet Table 9, there is a description of 2.8V in the SVNS only mode in Table12.

=> http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Which is the minimum value?

Q2)

When using with PMIC (MMPF0100F0AEP), in SNVS mode, Is setting change needed though the VSNVS output is 2.5V (default)?

Best Regards,

George

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,719件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

1. correct value gives datasheet Table 9 sect.4.1.3 Operating Ranges

2. MMPF0100 VSNVS output is 3.0V (default)

Table 10. Start-up Configuration

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,720件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

1. correct value gives datasheet Table 9 sect.4.1.3 Operating Ranges

2. MMPF0100 VSNVS output is 3.0V (default)

Table 10. Start-up Configuration

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,719件の閲覧回数
george
Senior Contributor II

Dear Igor,

Thank you for the comment about Question 1.

And, Q2 had a typo by me.

When using with PMIC (MMPF0100F0AEP), The VSNVS output is 2.5V in OFF mode.

QSB is such at when of PowerOFF.

However, the operating range of VDD_SNVS_IN is specified as 2.9V - 3.3V in datasheet Table 9.

=> http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Is it necessary to change setting into the range?

Best Regards,

George

0 件の賞賛
返信
1,719件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

one needs to have valid coincell connected to LICELL,

check MMPF0100 sect.6.4.7 VSNVS LDO/Switch

Best regards

igor

0 件の賞賛
返信
1,719件の閲覧回数
george
Senior Contributor II

Dear Igor,

It seems that my conditions description is not good.

I close here and I will Post it newly.

BR

George

0 件の賞賛
返信