Opencv facedetect lena.jpg on IMX6Q : detection time = 2506.65 ms

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Opencv facedetect lena.jpg on IMX6Q : detection time = 2506.65 ms

1,227 Views
hjpark71
Contributor III

Hi NXP,

I run Opencv "samples/c/facedetect lena.jpg" on Linaro-alip what is running on imx6q 800MHz.

it works well but the speed is so slow..

it is message from facedetect..

detection time = 2506.65 ms

do you think  2506.65 ms is normal on imx6q ?

or, Is there any way to improve the speed of opencv on imx6q?

Thanks and Best regards,

HJ

Labels (2)
0 Kudos
Reply
1 Reply

735 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi hj

2506ms for Facedetection is too much!, Please make sure that you are y using Opencv on ubuntu hardfloat rootfs.

Building OpenCV on ubuntu hardfloat rootfs for i.MX6Q

Fast GPU Image Processing in the i.MX 6x

Regards

0 Kudos
Reply