OpenJDK 64-Bit Server VM warning:

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

OpenJDK 64-Bit Server VM warning:

跳至解决方案
23,284 次查看
vinothkumars
Senior Contributor IV

Dear NXP,

Got following error while building android 9 automotive for IMX8 board. Please provide the fix for it,

OpenJDK 64-Bit Server VM warning: INFO: os::commit_memory(0x0000000761500000, 635437056, 0) failed; error='Not enough space' (errno=12)

 

Resolved by reboot. But, I need permanent solution.

 

 

Thanks & Regards,

Regards,
Vinothkumar Sekar
0 项奖励
回复
1 解答
23,275 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

The following suggestions are for your reference:
1. Linux Ubuntu host has at least 16GB Memory.
2. Linux Ubuntu host has at least 300GB hard disk space.
3. If the ubuntu host has 16GB memory, you can compile with 4 threads at most; if the compilation threads are greater than 4, there may still be insufficient memory

Hope above information is helpful to you.

Have a nice day!

B.R,

weidong

在原帖中查看解决方案

2 回复数
23,276 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

The following suggestions are for your reference:
1. Linux Ubuntu host has at least 16GB Memory.
2. Linux Ubuntu host has at least 300GB hard disk space.
3. If the ubuntu host has 16GB memory, you can compile with 4 threads at most; if the compilation threads are greater than 4, there may still be insufficient memory

Hope above information is helpful to you.

Have a nice day!

B.R,

weidong

23,252 次查看
vinothkumars
Senior Contributor IV

Thank you weidong_sun

 

You are right my local desk D have less than the 300 GB. after freed I got resolved from this.

Linux Ubuntu host has at least 300GB hard disk space.

 

Regards,

Regards,
Vinothkumar Sekar
0 项奖励
回复