OpenGL and OpenVG in Windows Embedded Compact 7 on imx53 platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenGL and OpenVG in Windows Embedded Compact 7 on imx53 platform

3,733件の閲覧回数
seetha
Contributor III

Hi all,

I am working in Wince 7 on imx53 platform. Now everything is working fine.I want to run some OpenGL and OpenVG applications on my platform.Does anybody know about this. Does anybody have done it earlier, if so please give me a clue to do the same on ma platform.If anybody has any sample apps of OpenVG and OpenGL for windows Embedded Compact 7 please let me know.

Thanks and Regards,

Seetharam

ラベル(1)
タグ(2)
0 件の賞賛
返信
5 返答(返信)

2,138件の閲覧回数
iMXAndrew
Contributor II
0 件の賞賛
返信

2,138件の閲覧回数
PrabhuSundarara
NXP Employee
NXP Employee

Hi Deepak,

I noticed another thread http://imxcommunity.org/group/wince/forum/topic/show?id=4103961%3ATopic%3A58704&xg_source=msg where the CPU is only 40%. Did you figured out the issue?

0 件の賞賛
返信

2,138件の閲覧回数
DeepakNaik
Contributor I

Hello Prabhu,

I executed the "opengles20_traingle_test.exe as tiger.exe,on SABRE/WinCE7 and QSB/WinCE7 platform. CPU utlisation goes 100 %.

Are we missing any configuration (GPU)?

 

Thanks & Regards,

Deepak

0 件の賞賛
返信

2,138件の閲覧回数
seetha
Contributor III

Thanks Prabhu for your replay. All the applications you mentioned are working fine. Thanks a lot again.

Regards,

Seetharam

0 件の賞賛
返信

2,138件の閲覧回数
PrabhuSundarara
NXP Employee
NXP Employee

Hi Seetharam,

WinCE 7 bsp is preloaded with sample applications. You can try

es11ex_driverTest.exe for OpenGL ES 1.1

opengles20_triangle_test.exe for OpenGL ES 2.0

tiger.exe for OpenVG.

 

Br,

Prabhu

0 件の賞賛
返信