OpenGL ES 3.0 support status by i.MX6 Series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenGL ES 3.0 support status by i.MX6 Series

Jump to solution
3,686 Views
norishinozaki
Contributor V

Hello, Champs,

I'm checking OpenGL ES versions supported by i.MX6 series per customer's request.

I'm referring to Reference Manuals and the "i.MX Family Comparison Chart" linked in below.

http://cache.freescale.com/files/32bit/doc/brochure/FLYRIMXPRDCMPR.pdf

In this chart, OpenGL ES 3.0 is supported by Quad, Dual,DualLite, Solo.

However in each Reference Manual,

Quad/Dual : No mention for 3.0

DL/Solo   : OpenGL ES 1.1, 2.0, and 3.0 (draft)

1. What is the real status of the ES 3.0 support?

2. Is there any schedule for ES 3.1?

Best regards,

Nori Shinozaki

Labels (2)
Tags (3)
0 Kudos
1 Solution
1,052 Views
norishinozaki
Contributor V

Hello Igor,

Thank you, I understood ES 3.0 will be supported in i.MX6 which has GC2000 or GC880 inside.

Best regards,

N.Shinozaki

View solution in original post

0 Kudos
2 Replies
1,052 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

you can look at attached document for current yocto OpenGL support.

OpenGL ES 3.0 will be supported on next release with linux 3.10.31

Freescale OpenEmbedded/Yocto Layers discussion list ()

I am not aware of plans for OpenGL ES 3.1.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,053 Views
norishinozaki
Contributor V

Hello Igor,

Thank you, I understood ES 3.0 will be supported in i.MX6 which has GC2000 or GC880 inside.

Best regards,

N.Shinozaki

0 Kudos