OpenCv error in IMX8QXP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenCv error in IMX8QXP

2,051件の閲覧回数
diwakar2599
Contributor II

Hi,

I am getting the below error when I try to run the NXP eIQ Machine Learning by OpenCV(4.2.0)

 

terminate called after throwing an instance of [947.599867] audit: type=1701 audit (16 83731664.936:7): auid=4294967295 uid=0 gid=0 ses=4294967295 pid= 1060 comm="example_dnn_obj" exe="/usr/share/OpenCV/samples/bin/example_dnn_object_detection" sig-6 res=1

cv::Exception'

what(): OpenCV (4.2.0) /usr/src/debug/opencv/4.2.0.imx-re/git/modules/core/src/persistence.cpp:719: error: (-49: Unknown error code -49) Input file is invalid in function 'open'

Aborted

 

please help me to solve this issue.

0 件の賞賛
返信
4 返答(返信)

2,022件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
 
My apology for the delayed response.
Kindly share the steps you followed to reproduce the issue at our end.
 
Thanks & Regards
Dhruvit Vasavada
0 件の賞賛
返信

2,009件の閲覧回数
diwakar2599
Contributor II
Hi @Dhruvit

For YOLO object detection I am facing the issue
I just run the following command for object detection

./example_dnn_object_detection -width=1024 -height=1024 -scale=0.00392 -input=dog416.png -
rgb -zoo=models.yml yolo
0 件の賞賛
返信

1,984件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @diwakar2599,

I hope you are doing well
 
There could be an issue in the particular source file. Kindly try to download that file from the git.
The error may also come due to the invalid XML file. Please check the same.
 
Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信

1,978件の閲覧回数
diwakar2599
Contributor II
Hi @Dhruvit

I will try and update the result soon
0 件の賞賛
返信