I've built Linux for an i.MX6 SABRE as per the "i.MX Yocto Project User's Guide". It includes opencv but there is a "contrib" folder not present which I would like to use as it is in an old application which I am trying to cross-compile for the SABRE. Is there a way to add this to the Yocto build?
已解决! 转到解答。
Hi,
The folder “contrib” depends of the OpenCV version. You could take a look at the following links for additional details:
https://docs.opencv.org/trunk/d7/d9f/tutorial_linux_install.html
https://community.nxp.com/docs/DOC-331941
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for that info Carlos.
The functions from contrib are located in different libraries in the later versions of OpenCV, so the solution was to amend the include paths to where these functions are now located.
Hi,
The folder “contrib” depends of the OpenCV version. You could take a look at the following links for additional details:
https://docs.opencv.org/trunk/d7/d9f/tutorial_linux_install.html
https://community.nxp.com/docs/DOC-331941
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------