Hello:
I have some products that are in production with the Freescale i.MX31 and i.MX53 processors. When we released these products, there were no Open GL drivers.
Are there Open GL drivers available now for either or both of these processors and if so, where can I get them?
Thanks!
Paul
Hi Paul
drivers can be found in BSPs on links below (please look at description in attached docs)
L2.6.35_11_09_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation
11.09. Supports MCIMX53-START and MCIMX53-START-R.
IMX31_PDK15_LINUX_BSP : Linux 2.6.26 Source Code Files for Release 1.5.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------