Once my application is developed can I use the SOM in another system?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Once my application is developed can I use the SOM in another system?

611件の閲覧回数
RodneyFulk
Contributor III

I am looking for something simple like the i.MX 53QSB but this looks somewhat interesting.


At this time I am just a Digital Media Software Engineering student and I have a pet project I am researching right now.


I believe the i.MX6 platform is the right one to use but I am unsure of how this all fits together. I am a newbie to this and was turned to Freescale during a tour of a local Automotive Contractor that is developing some uses with the i.MX53 QSB. After seeing what they are using it for and where they are going with it I started looking but I think for my application the MX6 is more likely the way to go.

I am considering purchasing the i.MX6 SOM and Development board but I am curious how to actually put this into another board for actual usage. In my project I will be using this to interface into a 2003 Chevy Avalanche and will want to hide it away in the dash in as small of a package as possible. The plan is to use the i.MX6 as the central brain to a sophisticated Alarm and Convenience system that will control many things and use things such as Bluetooth, GPS, ODBII, WiFi to communicate with other devices and potentially provide things such as GPS tracking, automatic starting etc etc. The User interface will be through a 7" touch screen incorporated into an over head console.  To do some of the interfacing I will likely be utilizing a secondary system such as an Arduino or Parallax Propeller to actually connect to the Vehicle when it requires Relays or other controllers to interface into the vehicle its self which will in turn be controlled by the i.MX6 processor.


When I am finished with the development of this how do I move this SOM to an installable system? Or is the development board designed to be used as the actual "production" board as well?

I am unsure how to connect this to the secondary board at this time but I will work on that once I have the unit in my hand. The Arduino and Propeller systems really can go just about any route. CAN, I2C, Serial... I am more of a medium grade programmer and beginner where hardware is concerned.

ラベル(1)
0 件の賞賛
1 返信

548件の閲覧回数
PradapRaj
Contributor III

For your Application, i feel 53QSB like solution may not workout. Because your application requires specific interfaces which need to be interfaced to CPU and with 53QSB you may not be able to interface all the modules.

i.MX6 SOM gives you the modular solution, because it takes out of complex part of high end CPU design from the user and provides the full flexibly & easiest way for user to design only low complex 2/4 layer board with user specific interfaces/modules. Also since Qseven SOM pinouts are pre defined standard, user can upgrade their systems in future with new latest high end CPU by only replacing the SOM without affecting the entire systems.Since SOM is coming with fully tested BSP software support, user no need worry on complex CPU & memory related  drivers/software and user has to only look on their application specific drivers/software which gives user quick time to market.

i.MX6 SOM Development platform gives you the immediate solution with predefined interfaces. This Nano-ITX form factor developement platform supports most of the interfaces you required [like 7" LCD, SD wifi port(Optional), UART port for GPS (Optional), Bluetooth through USB] and gives you the compact solution.For more details on SOM and Developement platform, please send mail to mktg@iwavesystems.com or provide your mailid.

0 件の賞賛