On IPU Base address in imx6qdl.dtsi

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

On IPU Base address in imx6qdl.dtsi

跳至解决方案
1,661 次查看
gaun
Contributor II

Hi,

Is there a typo in the in the base address of the IPU in imx6qdl.dtsi? The base address should have been 0x02600000 and not 0x02400000, right?

For reference:

linux-fslc/imx6qdl.dtsi at patches-4.1 · Freescale/linux-fslc · GitHub

I verified in the reference manuals and I don't find the IPU memory map at 0x02400000. Please verify.

Thanks.

标签 (4)
0 项奖励
回复
1 解答
1,517 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following

About imx6d ipu base address different in RM. and device tree.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,518 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following

About imx6d ipu base address different in RM. and device tree.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复