On IMX8MP LVDS display with 6.1 kernel is not working which is working on 5.15 kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

On IMX8MP LVDS display with 6.1 kernel is not working which is working on 5.15 kernel

跳至解决方案
7,324 次查看
Chandrasekhar-carrier
Contributor II

Hi Team, we are able to bring-up the LVDS display on 5.15 kernel on imx8mp custom board, but when we are porting from 5.15 to 6.1 kernel LVDS display is not working.

Below are the panel modifcations added:

With the same below modfications display is working in 5.15 kernel. So need supoort to bringup the display.

drivers/gpu/drm/panel/panel-simple.c | 97 ++++++++++++++++++++++++++++
1 file changed, 97 insertions(+)

diff --git a/drivers/gpu/drm/panel/panel-simple.c b/drivers/gpu/drm/panel/panel-simple.c
index b73669808347..605dce99d1ab 100644
--- a/drivers/gpu/drm/panel/panel-simple.c
+++ b/drivers/gpu/drm/panel/panel-simple.c
@@ -2128,6 +2128,94 @@ static const struct panel_desc hitachi_tx23d38vm0caa = {
},
};

+static const struct display_timing auo_g156han04_0_timings = {
+ .pixelclock = { 141000000, 141000000, 141000000 },
+ .hactive = { 1920, 1920, 1920 },
+ .hfront_porch = { 60, 60, 60 },
+ .hback_porch = { 60, 60, 60 },
+ .hsync_len = { 64, 64, 64 },
+ .vactive = { 1080, 1080, 1080 },
+ .vfront_porch = { 12, 12, 12 },
+ .vback_porch = { 12, 12, 12 },
+ .vsync_len = { 12, 12, 12 },
+};
+
+static const struct panel_desc auo_g156han04_0 = {
+ .timings = &auo_g156han04_0_timings,
+ .num_timings = 1,
+ .bpc = 8,
+ .size = {
+ .width = 344,
+ .height = 194,
+ },
+ .delay = {
+ .prepare = 10,
+ .enable = 50,
+ .disable = 50,
+ .unprepare = 200,
+ },
+ .bus_format = MEDIA_BUS_FMT_RGB888_1X24,
+};
+
+static const struct display_timing lxd_m773a_timings = {
+ .pixelclock = { 60000000, 60000000, 60000000 },
+ .hactive = { 1024, 1024, 1024 },
+ .hfront_porch = { 40, 40, 40 },
+ .hback_porch = { 40, 40, 40 },
+ .hsync_len = { 20, 20, 20 },
+ .vactive = { 600, 600, 600 },
+ .vfront_porch = { 20, 20, 20 },
+ .vback_porch = { 20, 20, 20 },
+ .vsync_len = { 10, 10, 10 },
+};
+
+static const struct panel_desc lxd_m773a = {
+ .timings = &lxd_m773a_timings,
+ .num_timings = 1,
+ .bpc = 8,
+ .size = {
+ .width = 154,
+ .height = 85,
+ },
+ .delay = {
+ .prepare = 10,
+ .enable = 50,
+ .disable = 50,
+ .unprepare = 200,
+ },
+ .bus_format = MEDIA_BUS_FMT_RGB888_1X24,
+};
+
+static const struct display_timing lxd_m776a_timings = {
+ .pixelclock = { 60000000, 60000000, 60000000 },
+ .hactive = { 1024, 1024, 1024 },
+ .hfront_porch = { 40, 40, 40 },
+ .hback_porch = { 40, 40, 40 },
+ .hsync_len = { 20, 20, 20 },
+ .vactive = { 600, 600, 600 },
+ .vfront_porch = { 20, 20, 20 },
+ .vback_porch = { 20, 20, 20 },
+ .vsync_len = { 10, 10, 10 },
+};
+
+static const struct panel_desc lxd_m776a = {
+ .timings = &lxd_m776a_timings,
+ .num_timings = 1,
+ .bpc = 8,
+ .size = {
+ .width = 222,
+ .height = 125,
+ },
+ .delay = {
+ .prepare = 10,
+ .enable = 50,
+ .disable = 50,
+ .unprepare = 200,
+ },
+ .bus_format = MEDIA_BUS_FMT_RGB888_1X24,
+};
+
+
static const struct drm_display_mode innolux_at043tn24_mode = {
.clock = 9000,
.hdisplay = 480,
@@ -4201,6 +4289,15 @@ static const struct of_device_id platform_of_match[] = {
.compatible = "hit,tx23d38vm0caa",
.data = &hitachi_tx23d38vm0caa
}, {
+ .compatible = "lxd,m773a",
+ .data = &lxd_m773a,
+ }, {
+ .compatible = "lxd,m776a",
+ .data = &lxd_m776a,
+ }, {
+ .compatible = "auo,g156han04_0",
+ .data = &auo_g156han04_0,
+ }, {
.compatible = "innolux,at043tn24",
.data = &innolux_at043tn24,
}, {
--
2.34.1

 

Here is the DTS file used:

/ {
lvds0_panel {
status = "okay";
compatible = "lxd,m776a";
backlight = <&lvds_backlight>;
enable-gpios = <&gpio1 13 GPIO_ACTIVE_HIGH>;
port {
panel_lvds_in: endpoint {
remote-endpoint = <&lvds_out>;
};
};
};
lvds_backlight {
enable-gpios = <&gpio1 0 GPIO_ACTIVE_HIGH>;
};
// gpio3_IO23 on lec-imx8mp is display mux
reg_mipi_lvds_select: regulator-mipi-lvds {
compatible = "regulator-fixed";
regulator-name = "mipi_lvds_select_vbus";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_disp_select>;
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
gpio = <&gpio3 23 GPIO_ACTIVE_HIGH>;
enable-active-low;
regulator-always-on;
};
};


&ldb {
status = "okay";
//fsl,dual-channel;
lvds-channel@0 {
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
status = "okay";
/delete-node/ port@1;
port@1 {
reg = <1>;
lvds_out: endpoint {
remote-endpoint = <&panel_lvds_in>;
};
};
};
};
&ldb_phy {
status = "okay";
};
&i2c3 {
touchscreen@41 {
compatible = "ilitek,ili251x";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_touch_en &pinctrl_touch_rst>;
reg = <0x41>;
interrupt-parent = <&gpio1>;
interrupts = <0 IRQ_TYPE_EDGE_FALLING>;
reset-gpios = <&gpio1 7 GPIO_ACTIVE_HIGH>;
touchscreen-inverted-x;
touchscreen-inverted-y;
};
};

@griffin.peterson@nxp.com, @JainthKumar.B@Carrier.com

0 项奖励
回复
1 解答
6,591 次查看
Chandrasekhar-carrier
Contributor II

after adding the below flags in the panel_desc then display is working as expected

 

.bus_format = MEDIA_BUS_FMT_RGB888_1X7X4_SPWG,
.bus_flags = DRM_BUS_FLAG_DE_HIGH,
.connector_type = DRM_MODE_CONNECTOR_LVDS,

在原帖中查看解决方案

0 项奖励
回复
7 回复数
6,592 次查看
Chandrasekhar-carrier
Contributor II

after adding the below flags in the panel_desc then display is working as expected

 

.bus_format = MEDIA_BUS_FMT_RGB888_1X7X4_SPWG,
.bus_flags = DRM_BUS_FLAG_DE_HIGH,
.connector_type = DRM_MODE_CONNECTOR_LVDS,

0 项奖励
回复
7,280 次查看
Chandrasekhar-carrier
Contributor II

There are no error messages, but display is not coming as expected

Chandrasekharcarrier_0-1719937688455.png


Is there any clock related changes we need to add in 6.1 Kernel?? or any other suggestions.

0 项奖励
回复
7,294 次查看
Chandrasekhar-carrier
Contributor II

hi @joanxie 

The Display backlight is initializing but on the display output is coming like below

Chandrasekharcarrier_0-1719933913035.png



So unable to figure out what modifications went wrong 



0 项奖励
回复
7,278 次查看
joanxie
NXP TechSupport
NXP TechSupport

did you change any source code in the 5.15? did you just use the default lvds driver? as I known, current bsp couldn't support 60Mhz lvds display(single channel) as default, you need change the source code, if you change the 5.15 bsp, did you change corresponding to the 6.1?

0 项奖励
回复
7,267 次查看
Chandrasekhar-carrier
Contributor II
We didn't do any bsp changes except the panel detail structures are added in 5.15 kernel. So did the same modifications in the 6.1 kernel as well
0 项奖励
回复
7,233 次查看
joanxie
NXP TechSupport
NXP TechSupport

do you mind dumping the clock to check? could you get the correct clock for your lvds panel, I checked the ldb driver, I don't find anything change would affect your display

0 项奖励
回复
7,299 次查看
joanxie
NXP TechSupport
NXP TechSupport

what do you mean "not working"?do you get anything error messages?

0 项奖励
回复