OV5640 for imx8mpevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OV5640 for imx8mpevk

Jump to solution
1,390 Views
Mawriyo
Contributor I

Where can I find a n OV5640 for the IMX8MPEVK dev board that can fit in the MIPI CSI port? Can't seem to find it.

0 Kudos
Reply
1 Solution
1,385 Views
khang_letruong
Senior Contributor III

Hi,

Just in case you have an EVK from NXP, take a look at this : https://www.nxp.com/part/MINISASTOCSI#/

The OV5640 sensor is quite popular. Most of NXP partners (TechNexion, Variscite, ...) also have the OV5640 camera module that is suitable for their SoM/Carrier Board.

Regards,

K.

View solution in original post

4 Replies
1,340 Views
Mawriyo
Contributor I

Seems like I got one of the cameras to work but the module does not seem to work for csi port 2 . Is there a DTB that supports for a duel camera for this module.

0 Kudos
Reply
1,325 Views
khang_letruong
Senior Contributor III

Hi @Mawriyo ,

You can do it yourselves by inspiring the following dts :

arch/arm64/boot/dts/freescale/imx8mp-evk-dual-basler.dts
arch/arm64/boot/dts/freescale/imx8mp-evk-dual-ov2775.dts

Moreover, in your previous question, I also shared a discussion related to dual ov5640 : https://community.nxp.com/t5/i-MX-Processors/Dual-OV5640-cameras-on-iMX8M-Plus/m-p/1250820

Regards,
K.

0 Kudos
Reply
1,386 Views
khang_letruong
Senior Contributor III

Hi,

Just in case you have an EVK from NXP, take a look at this : https://www.nxp.com/part/MINISASTOCSI#/

The OV5640 sensor is quite popular. Most of NXP partners (TechNexion, Variscite, ...) also have the OV5640 camera module that is suitable for their SoM/Carrier Board.

Regards,

K.

1,381 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good

0 Kudos
Reply