Hi,
I'm debugging our OV5640 camera module on our new i.MX93 board with BSP version LF-6.1.22-2.0.0, it works fine on our some other boards based on i.MX8MN, i.MX8MM, i.MX8MQ, i.MX8ULP.
Refer to this post About settings to operate ov5640 camera on i.MX93EVK, it works on resolutions 1920x1080, 640x480, 320x240..., but can not work on 2592x1944, 1280x720, 1024x768, 720x480. Attachment is the capture images with those resolutions.
root@maaxboardosm93:~# v4l2-ctl -d0 --list-framesizes YUYV
ioctl: VIDIOC_ENUM_FRAMESIZES
Size: Discrete 160x120
Size: Discrete 176x144
Size: Discrete 320x240
Size: Discrete 640x480
Size: Discrete 720x480
Size: Discrete 720x576
Size: Discrete 1024x768
Size: Discrete 1280x720
Size: Discrete 1920x1080
Size: Discrete 2592x1944
Below is our DTS configuration for MIPI-CSI and image sensor.
/ {
... ...
/* It's a 25MHz crystal oscillator on OV5640 camera board */
cam_xtal: cam-xtal {
compatible = "fixed-clock";
#clock-cells = <0>;
clock-frequency = <25000000>;
clock-output-names = "cam_xtal";
};
... ...
};
&lpi2c5 {
... ...
ov5640_mipi: ov5640_mipi@3c {
compatible = "ovti,ov5640";
reg = <0x3c>;
clocks = <&cam_xtal>;
clock-names = "xclk";
powerdown-gpios = <&ioexpander1 6 GPIO_ACTIVE_LOW>;
reset-gpios = <&ioexpander1 7 GPIO_ACTIVE_LOW>;
status = "okay";
port {
ov5640_mipi_ep: endpoint {
remote-endpoint = <&mipi_csi_ep>;
data-lanes = <2>;
cfg-clk-range = <28>;
hs-clk-range = <0x16>;
};
};
};
};
&epxp {
status = "okay";
};
&media_blk_ctrl {
status = "okay";
};
&cameradev {
status = "okay";
};
&isi_0 {
status = "okay";
cap_device {
status = "okay";
};
};
&mipi_csi {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
port@0 {
reg = <0>;
mipi_csi_ep: endpoint {
remote-endpoint = <&ov5640_mipi_ep>;
data-lanes = <2>;
cfg-clk-range = <28>;
hs-clk-range = <0x16>;
bus-type = <4>;
};
};
};
Can anyone give us some guide to support all those resolutions ? Thanks in advanced!
Same error I am getting in Android 11 , imx8mm
Camera - OV5640 MIPI-CSI
Display - 6 Inch MIPI-DSI
How to solve this ?
@joanxie please post the solution here.That will be usefull for others also.
Hi @joanxie
Thanks for your reply! Below is the "media-ctl -p" command output:
root@maaxboardosm93:~# media-ctl -p
Media controller API version 6.1.22
Media device information
------------------------
driver mxc-md
model FSL Capture Media Device
serial
bus info platform:42800000.bus:camera
hw revision 0x0
driver version 6.1.22
Device topology
- entity 1: mxc_isi.0 (16 pads, 2 links)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
<- "mxc-mipi-csi2.0":4 [ENABLED]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Sink
pad5: Sink
pad6: Sink
pad7: Sink
pad8: Sink
pad9: Sink
pad10: Sink
pad11: Sink
pad12: Source
-> "mxc_isi.0.capture":0 [ENABLED]
pad13: Source
pad14: Source
pad15: Sink
- entity 18: mxc_isi.0.capture (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video0
pad0: Sink
<- "mxc_isi.0":12 [ENABLED]
- entity 22: mxc-mipi-csi2.0 (8 pads, 2 links)
type Node subtype V4L flags 0
device node name /dev/v4l-subdev0
pad0: Sink
<- "ov5640 4-003c":0 [ENABLED,IMMUTABLE]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Source
-> "mxc_isi.0":0 [ENABLED]
pad5: Source
pad6: Source
pad7: Source
- entity 31: ov5640 4-003c (1 pad, 1 link)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev1
pad0: Source
[fmt:UYVY8_1X16/160x120@1/15 colorspace:srgb xfer:srgb ycbcr:601 quantization:full-range
crop.bounds:(0,0)/2624x1964
crop:(16,14)/2592x1944]
-> "mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE]
And I use "gst-launch-1.0" command to capture images, and below is my capture shell script.
#!/bin/bash
WORK_PATH=/tmp
IMG_PRFIX=capture_
# Check support resolutions: v4l2-ctl -d0 --list-framesizes YUYV
width=(2592 1920 1280 1024 720 720 640 320 176 160)
height=(1944 1080 720 768 576 480 480 240 144 120)
nums=${#width[@]}
cd $WORK_PATH
rm -f ${IMG_PRFIX}*.jpg
for ((i = 0; i < nums; i++)); do
w=${width[i]}
h=${height[i]}
echo ""
echo "Capture ${w}x${h} jpg image"
gst-launch-1.0 v4l2src device=/dev/video0 num-buffers=1 ! video/x-raw,format=YUY2,width=${w},height=${h} ! jpegenc ! filesink location=${IMG_PRFIX}${w}x${h}.jpg
done
sz ${IMG_PRFIX}*.jpg
@joanxie @wenxue_guo
mail me too , I am also facing the same problem.