Hi,
I'm using a OmniVision OV5640 MIPI-CSI2 image sensor with a iMX6 Quad board.
I have seen in the datasheets that 720p60 capture can be done using OV5640. However, the drivers does not seem to support 60 fps capture? What changes must be done to obtain 60 fps capture?
Hi Abhishek
please look for answer on below link
OV5640 MIPI-CSI2 driver - why the limitations?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I had gone through that link. Yuri has posted that " it is required to create / support special command sequences (tables) to program
a camera (say, via I2C) for different modes / frame frequencies". Can you elaborate on this.
I had also gone through the discussion on the meta-freescale mailing list. But I could not find the required solution. In the discussion on the on the meta-freescale mailing list, I read about changing i2c blobs . I am not aware of it.
What are the changes required for 60 fps capture?
Hi Abhishek
seeems these commands are proprietary OmniVision
so would suggest to apply to OmniVision tech support.
Best regards
igor