OV5640 ISP porting to imx8mp-lppddr4-evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OV5640 ISP porting to imx8mp-lppddr4-evk

799 Views
gowrish
Contributor I

Hello NXP community,

Could you please let me know whether OV5640 porting via ISP on imx8mp-lppddr4-evk  is supported or not.

If yes, please let me know what are the dependencies or supported packages need to be add/create .

In AN13713 document there are some steps related to ISP porting but i see that is with respect to other sensor not ov5640, If you confirm that if i follow the steps mentioned in AN13713 i could port ov5640 via isp to imx8mp then i'll follow that.

Screenshot from 2024-07-15 12-13-24.png

Also please provide any document specifically for ov5640 porting via ISP to imx8mp lpddr4 evk.

If no document please provide detailed steps possible.

 

Thanks in Advance,

 

Regards,

Gowrish.

0 Kudos
Reply
3 Replies

752 Views
pengyong_zhang
NXP Employee
NXP Employee
0 Kudos
Reply

765 Views
gowrish
Contributor I

Hi @pengyong_zhang ,

 

Thanks for the reply.

Through ISI it is working fine I want to know how to enable the ISP porting to OV5640 camera only in .dts any supported packages are there ?

Thanks & Regards,

Gowrish.

0 Kudos
Reply

776 Views
pengyong_zhang
NXP Employee
NXP Employee

HI @gowrish 

Could you please let me know whether OV5640 porting via ISP on imx8mp-lppddr4-evk  is supported or not.

A : It supports.

boot with imx8mp-evk-ov2775-ov5640.dtb file.  set status of &isi_0 or &isi_1 to “Okay” in the dts file

0 Kudos
Reply