OV5640 Auto focus support for Linux 3.10.53

cancel
Showing results for 
Search instead for 
Did you mean: 

OV5640 Auto focus support for Linux 3.10.53

509 Views
mohamedsarjoond
Contributor III

Dear Team,

I am using OV5640 color CMOS 5MP camera(2592x1944) I want to enable auto focus on the driver. Just want to know whether auto focus drivers/steps is available in Linux 3.10.53 kernel. If not in 3.10.53 and available in other linux releases means please share the reference code. I am currently stuck up with Auto focus enabling

Please help with this

Thanks & Regards

Sarjoon

0 Kudos
2 Replies

119 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Sarjoon

seems this feature is supported in boundary devices android

as mentioned on

OV5640 Auto Focus Drivers 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

119 Views
mohamedsarjoond
Contributor III

Dear Igor,

Thanks for the link. How can I get the source code of the ov5640.c, I dont want to download the full source it will take days for me to download, since I dont have much time. Any  ov5640 source code alone will be helpful. Can you please share the source code of ov5640 with auto focus support done ?

It will be a lot helpful for me.

Thanks in advance

Sarjoon

0 Kudos