OTP problem of imx7ulp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTP problem of imx7ulp

1,249 Views
stanley_yeh
Contributor II

Hi there,

I am using i.MAX7ULP and try to use u-boot commands to program OTP memory.

The command is "fuse prog 0 0 0x55667788". (bank: 0, word: 0, val: 0x55667788)

However, when I use sense command to read the OTP memory, the value is 0x00007788.

I also programmed other words of bank 0, I got the same result.

Finally, I programmed the 7th word of bank 30 with "fuse prog 30 7 0x55667788" command, the return value is normal.

Could you tell me why, please? I have no idea about this problem.

Thanks a lot.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,137 Views
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX7ULP is not launched yet and is not supported in i.MX Community.

Please create request \ ticket, using Your corporate e-mail as account.

Support|NXP 

Regards,

Yuri.

0 Kudos
Reply