OTP config on PMIC NF0100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTP config on PMIC NF0100

901 Views
christophe
Contributor V

Hi,

On MCIMX6Q-SDB Sabre board: could be possible to obtain from Freescale full OTP configuration used into PMIC (not only voltages or startup times as depicted in F0,F1 or F2 datasheet config, but especially all other configurated OTP stuffs in Sabre board). It will be helpful for us to compare our OTP config, before order pre-programmed pmic to Freescale.

Thanks.

CC

0 Kudos
Reply
2 Replies

618 Views
AnandBalakrishn
Contributor V

Hello Christophe,

Everything that is 'OTP-able' on the MMPF0100 is listed in Table 9 of the datasheet. What specifically are you looking for?

If you could send your OTP configuration, I can do a cross check to make sure it matches our standard flavors.

Regards,

Anand


0 Kudos
Reply

618 Views
christophe
Contributor V

No, at the end i will use a standard OTP config F0. The doubt is removed on this point.

Thanks.

0 Kudos
Reply