OTA update process in iMX8MP evk board running Android 14

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OTA update process in iMX8MP evk board running Android 14

359件の閲覧回数
Manoj_Kumar
Contributor II

Hello @Harvey021 

 

These are our requirements regarding OTA update process.
    1. The software should implement Secure Boot to verify software authenticity.
    2. The software should support secure OTA updates with encryption.
 
As per the requirement we have completed Secure boot with HABv4 to get signed images and the board is booting fine without any hab events. Now we need to do secure OTA updates with encryption.
 
In Android user’s guide
In section 7.1.6.3 Building an OTA package with encrypted boot
It is mentioned that,
Move the encrypted target SPL and bootloader images to the directory of ${MY_ANDROID}/out/target/product/${TARGET_PRODUCT}/obj/UBOOT_COLLECTION/. Override the original target files.
 
Execute the following command to generate an OTA package, which includes the encrypted SPL and bootloader images.
$ ./imx-make.sh kernel -j4
$ BUILD_ENCRYPTED_BOOT=true make otapackage -j24 IMX_OTA_POSTINSTALL=1
 
Then the OTA package includes the encrypted SPL and bootloader images. Besides the OTA package, DEK Blobs of SPL and bootloader images need to be provisioned into the device before applying the OTA package.
 
Here what process we need to follow?
If we copy the signed images generated in the secure boot with HABv4 into the directory of  ${MY_ANDROID}/out/target/product/${TARGET_PRODUCT}/obj/UBOOT_COLLECTION/ and generate the OTA package will fulfill our both requirements?
 
If yes, to generate OTA package can we use this command “BUILD_ENCRYPTED_BOOT=true make otapackage -j24 IMX_OTA_POSTINSTALL=1” or need to modify it to “make otapackage -j24 IMX_OTA_POSTINSTALL=1”?
 
If not, do we need to follow Encrypted boot with HABv4? But it will encrypt only the boot images, what about the encryption of the OTA update?
 
 
For implementing OTA update we are using “SystemUpdaterSample” application with “Lighttpd” server as mentioned in section “7.2.2 Using a customized application to update the Android platform”.
 
 
Best regards,
Manoj kumar
ラベル(1)
0 件の賞賛
返信
1 返信

320件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi  @Manoj_Kumar 

BUILD_ENCRYPTED_BOOT cannot be deleted. Without it, the encrypted bootloader will not be compiled into the OTA package. You need to follow the Encrypted boot with HABv4 and then follow the normal OTA process.

 

Regards

Harvey

0 件の賞賛
返信