Dear all,
We use FSL LTIB Linux.
Linux: L3.0.35_4.0.0_ER_SOURCE_BSP
We analyse OSS about our system based on this.
The following library is included in FSL LTIB Linux.
However, the source code of these libraries is not offered.
Do these violate OSS?
If they violate OSS, would you tell me the maker providing these?
Function Library name Package
OpenGL gpu-viv-bin-mx6q gpu-viv-bin-mx6q-3.0.35-
EGL gpu-viv-bin-mx6q gpu-viv-bin-mx6q-3.0.35-
firmware-imx firmware-imx firmware-imx-3.0.35-4.0.
base_libs base_libs base_libs-1.2-1
imx-lib imx-lib imx-lib-3.0.35-4.0.0
Best Regards,
Yuuki
Solved! Go to Solution.
Dear all,
We have an additional question.
Would you answer about the following contents?
1)
When we download LTIB Linux, Agreement is displayed.
"FREESCALE SEMICONDUCTOR SOFTWARE LICENSE AGREEMENT"
Do the contents listed in Section 2.Licenses of Agreement apply to all libraries?
2)
We understood that the following library is LGPL license.
# ./ltib -mlistpkgs
----------------------- ---------------- ----------- ----------- -----------------------------------------
Package Spec file Enabled License Summary
----------------------- ---------------- ----------- ----------- -----------------------------------------
base_libs-1.2-1 base_libs y LGPL Base Libraries (from toolchain).
We use this library too.
We think that this library has to be shown a source code.
If our understanding is right, Would you offer the source code of this library?
3)
We use firmware-imx libraries.
This includes Atheros libraries.
We may use following drivers or libraries.
We think that we have to take out these licenses.
Would you tell me how to take out these licenses?
<drivers or libraries>
./ltib/rootfs/lib/modules/3.0.35-2508-g54750ff-MCXV-0x00000104/kernel/
drivers/net/wireless/ath
./ltib/rootfs/lib/modules/3.0.35-2508-g54750ff-MCXV-0x00000104/kernel/
drivers/net/wireless/ath/ath.ko
./ltib/rootfs/lib/modules/3.0.35-2508-g54750ff-MCXV-0x00000104/kernel/
drivers/net/wireless/ath/ath6kl
./ltib/rootfs/lib/modules/3.0.35-2508-g54750ff-MCXV-0x00000104/kernel/
drivers/net/wireless/ath/ath6kl/ath6kl.ko
./ltib/rootfs/lib/firmware/ath6k
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.0/athtcmd_ram.bin
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.0/athwlan.bin.z77
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.0/athwlan.bin
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw1.0/athwlan.bin.z77
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.1.1/athwlan_mobile.bin
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.1.1/athtcmd_ram.bin
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.1.1/athwlan.bin
./ltib/rootfs/lib/firmware/ath6k/AR6102/athwlan.bin.z77
Best Regards,
Yuuki