Currently I try to get an OPTEE enabled image to work on our custom iMX8QXP board with 1GB of RAM. I followed AN13275 as closely as possible (building ATF, SCFW, OP-TEE OS) and creating the final image with
make SOC=iMX8QX REV=C0 flash_spl_flexspi
U-Boot SPL 2022.04-dirty (Sep 26 2023 - 12:00:52 +0000)
Normal Boot
Trying to boot from SPI
Primary set selected
Load image from QSPI 0x52800
UU
and the following output from SCFW
Hello from SCU (Build 5624, Commit 6638c032, Nov 02 2022 07:45:49)
GS on SCU UART (G444) (build on Nov 9 2023 14:55:45)
board_get_ram_size() is 16
SCFW: DDR frequency = 1200000000
board_system_config(0, 0)
Start PMIC init
Finished PMIC init
board_set_power_mode(A35, 0, 0, 3)
ROM boot time = 57522 usec
Boot time = 55883 usec
Banner = 15054 usec
Init = 9169 usec
Config = 2838 usec
DDR = 12619 usec
SConfig = 2836 usec
Prep = 10727 usec
*** Debug Monitor ***
>$ NOTICE: Memreg 1 0x0 -- 0x1bffffff
NOTICE: Memreg 2 0x34000000 -- 0x37ffffff
NOTICE: Memreg 3 0x70000000 -- 0x7fffffff
NOTICE: Memreg 4 0x80000000 -- 0xffffffff
NOTICE: Memreg 5 0x400000000 -- 0x43fffffff
NOTICE: Non-secure Partitioning Succeeded
NOTICE: BL31: v2.6(release):OS026S00B12.OSQ-119-gbcc0f45ed7-dirty
NOTICE: BL31: Built : 14:55:42, Nov 9 2023
Afterwards I don't see any additional output. If I build ATF without optee support U-Boot SPL is successfully starting U-Boot. Can you give me any hints on how to debug this further?
解決済! 解決策の投稿を見る。
Hi
I got it working now. There where two remaining problems
make PLAT=imx8qx SPD=opteed BL32_BASE=0xbe000000 bl31
${CROSS_COMPILE}objcopy -O binary core/tee.elf tee.bin
I got this information from this description here.
I have now /dev/tee0 available when booting into linux.
Hi
I got it working now. There where two remaining problems
make PLAT=imx8qx SPD=opteed BL32_BASE=0xbe000000 bl31
${CROSS_COMPILE}objcopy -O binary core/tee.elf tee.bin
I got this information from this description here.
I have now /dev/tee0 available when booting into linux.
Just to note an additional finding:
Using tee-raw.bin from optee-os build works also but results in much smaller flash image. This also is in sync with optee-os-fslc.inc copying tee-raw.bin to DEPLOYDIR
Have you checked the <3. Allocate memory region for non-secure world.>?
If OP-TEE is implemented, the memory region 0xFE000000 – 0xFFFFFFFF is used by OP-TEE by default, in
case that the DRMA size is equal to or greater than 2 GB. This is set in arm-trusted-firmware/ plat/imx/imx8qx/
platform.mk with BL32_BASE and BL32_SIZE.
But if the new board’s DRAM size is less then 2 GB, then BL32_BASE need to be modified to highest memory address – BL32_SIZE. For example, if DRAM size is 1 GB, BL32_BASE is 0xBE000000.
Best regards
Harvey
Yes, I adapted ATF using the following patch.
diff --git a/plat/imx/imx8qx/platform.mk b/plat/imx/imx8qx/platform.mk
index c4028a8a9..fbf5366a4 100644
--- a/plat/imx/imx8qx/platform.mk
+++ b/plat/imx/imx8qx/platform.mk
@@ -49,7 +49,7 @@ $(eval $(call add_define,ENABLE_L2_DYNAMIC_RETENTION))
ifeq (${PLAT},imx8dx)
BL32_BASE ?= 0x96000000
else
-BL32_BASE ?= 0xfe000000
+BL32_BASE ?= 0xbe000000
endif
$(eval $(call add_define,BL32_BASE))
I then build ATF using the following command
make PLAT=imx8qx SPD=opteed bl31
My current BSP is based on lf-5.15.71-2.2.0