Hi:
My linux environment is ubuntu 18.04 64bit. When I download L5.10.9 BSP and attempt to compile imx-image-full. I find the onnxruntime recipes can not compile.
The error occur do_configure stage and below is the error.
| -- Performing Test HAS_TAUTOLOGICAL_POINTER_COMPARE
| -- Performing Test HAS_TAUTOLOGICAL_POINTER_COMPARE - Failed
| -- Performing Test HAS_CATCH_VALUE
| -- Performing Test HAS_CATCH_VALUE - Success
| -- Performing Test HAS_MISSING_BRACES
| -- Performing Test HAS_MISSING_BRACES - Success
| -- Performing Test HAS_IGNORED_ATTRIBUTES
| -- Performing Test HAS_IGNORED_ATTRIBUTES - Success
| -- Performing Test HAS_DEPRECATED_COPY
| -- Performing Test HAS_DEPRECATED_COPY - Success
| -- Performing Test HAS_DEPRECATED_DECLARATIONS
| -- Performing Test HAS_DEPRECATED_DECLARATIONS - Success
| -- Performing Test HAS_CLASS_MEMACCESS
| -- Performing Test HAS_CLASS_MEMACCESS - Success
| -- Performing Test HAS_MAYBE_UNINITIALIZED
| -- Performing Test HAS_MAYBE_UNINITIALIZED - Success
| -- Looking for clock_gettime in rt
| -- Looking for clock_gettime in rt - found
| -- The ASM compiler identification is GNU
| -- Found assembler: /home/duxy/L5.10.9/build-xwayland/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.5.3-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/aarch64-poky-linux-gcc
| CMake Warning at flake8.cmake:19 (message):
| Could not find 'flake8' to check python scripts. Please install flake8
| using pip.
| Call Stack (most recent call first):
| CMakeLists.txt:1449 (include)
|
Can anyone tell me how to solve this problem. Refer to the attachment for all logs