ODBS iMX28EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ODBS iMX28EVK

Jump to solution
1,514 Views
arunachalamrama
Contributor III

Hi,

I am running OBDS on iMX28EVK. NAND Test fails with output given below. Board has one MT29F4G16ABADAWP connected using NAND Flash Socket.

Any help on this?

Regards,

Arun

======================================================

---- Running < NAND > test

Please enter y or Y to confirm

input char is: y

Reset NAND

Read NAND ID for CE0: ID for CE0, is 0x2c, 0xdc, 0x90, 0x95, 0x56

**NAND device unrecognized!

======================================================

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,422 Views
igorpadykov
NXP Employee
NXP Employee

Hi Arun

supported parts are provided in file

include/mx28/supported_nand_parts.inl.

So please add necessary record for this NAND

and rebuild OBDS.

Best regards

igor

View solution in original post

4 Replies
1,422 Views
igorpadykov
NXP Employee
NXP Employee

Hi Arun

supported parts are provided in file

include/mx28/supported_nand_parts.inl

so one can add necessary record.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,422 Views
arunachalamrama
Contributor III

Hi igor,

I am using binary flashed on SD Card.

I have requirement to run OBDS and have the tests pass.

Please let me know steps / procedure to make OBDS NAND test pass on iMX28 EVK.

Regards,

Arun

0 Kudos
Reply
1,423 Views
igorpadykov
NXP Employee
NXP Employee

Hi Arun

supported parts are provided in file

include/mx28/supported_nand_parts.inl.

So please add necessary record for this NAND

and rebuild OBDS.

Best regards

igor

1,422 Views
arunachalamrama
Contributor III

Thanks, igor !

This helps.

Regards,

Arun

0 Kudos
Reply