Number of cycles needed to send a single pixel in RAW (Bayer) 12bit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Number of cycles needed to send a single pixel in RAW (Bayer) 12bit

跳至解决方案
1,913 次查看
ko-hey
Senior Contributor II

Hi all

I have a question about number of cycles needed to send a single pixel.

According to RM Rev3.0, there are following description.

pastedImage_0.png

How about RAW Bayer 12bit ?

Is it need 2 cyles/pixel ?

Ko-hey

标签 (2)
标记 (1)
0 项奖励
1 解答
1,443 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

yes this is right.

Best regards

igor

在原帖中查看解决方案

0 项奖励
8 回复数
1,443 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

for RAW Bayer 12bit it is 1 cycle/pixel

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
1,443 次查看
ko-hey
Senior Contributor II

Hi Igor

Thank you for reply but please let me confirm again.

According to the P2724 of RM Rev 3.0, there is a following description.

Bayer/Generic data = 1 cycle/pixel

However, in P2725 of RM Rev 3.0, there is a following description

Generic data = 2 cycle/pixel

Both of above description, I guess there have different parameters.

Could you check again ?

Ko-hey

0 项奖励
1,443 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

according to i.MX6DQ Datasheet (rev.4, 7/2015)

Table 66. Camera Input Signal Cross Reference, Format, and Bits Per Cycle

5,6 selection, it is 1 cycle.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

~igor

0 项奖励
1,443 次查看
ko-hey
Senior Contributor II

Hi Igor

I understand that the Generic data needs only 1 cycle from following description.

YCbCr, 16 bits-Supported as a "generic-data" input-with no on-the-fly processing.

Is this also same for RAW Bayer 12bit ?

Addition for this , is it same in both parallel and MIPI-CSIs I/F ?

Ko-hey

0 项奖励
1,443 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

according to RM for MIPI 1 cycle/pixel is for YUV422

2 cycle/pixel is for RAW (generic) format

1.jpg

Best regards

igor

0 项奖励
1,443 次查看
ko-hey
Senior Contributor II

Hi Igor

This is final confirm.

The following is the my understanding.

Is it correct ?

In parallel interface, Generic data needs 1 cycle/pixel

In MIPI-CIS2 interface, Generic data needs 2 cycle/pixel

I'm sorry for asking you many times.

But the cycle is very important for me.

Ko-hey

1,444 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

yes this is right.

Best regards

igor

0 项奖励
1,443 次查看
ko-hey
Senior Contributor II

Hi Igor

Thanks !

Ko-hey

0 项奖励