Number of SDRAM usage in EVKMIMXRT1170

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Number of SDRAM usage in EVKMIMXRT1170

ソリューションへジャンプ
1,449件の閲覧回数
Naresh_
Contributor II

We are working on an application development using EVKMIMXRT1170 for a 5 inch TFT display with RGB interface. With reference to the  EVK hardware design files(MIMXRT1170-EVK-design files-Rev C3),we are referring to the schematic file SPF-32171_C3 ,2 SDRAMs U13 and U25 are being placed in the EVK board. Each of the SDRAMs are 4 M *4 BANKS *16 bits SDRAM= 256Mbits. Are these SDRAMs are addressed using 16 bits data transfer (Read ,Write ) or 32 bit data transfer mode of usage . Also is it required to use both these SDRAMs in the EVK (U13 and U25) in building an application for TFT display interface.

Please let us know

0 件の賞賛
返信
1 解決策
1,443件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Naresh,

It is not required to use both SDRAM, you can use single SDRAM in your design.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,444件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Naresh,

It is not required to use both SDRAM, you can use single SDRAM in your design.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 件の賞賛
返信
1,432件の閲覧回数
Naresh_
Contributor II

Hello Felipe, Thank You for your reply

0 件の賞賛
返信