Not able to run same video application on imx-6 dual core as on ubuntu desktop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to run same video application on imx-6 dual core as on ubuntu desktop

537 Views
chewhouming
Contributor III

Hi

I am able to run Qt application on Ubuntu after inserting QT multimedia, multimediawidgets modules.

When i cross-compile and put the same application onto imx-6, it cannot run.

Like to ask for assistance.

Tags (1)
0 Kudos
1 Reply

469 Views
igorpadykov
NXP Employee
NXP Employee

Hi chew

i.MX should run optimized QT, please follow guidelines given in sect.5.6.7 Qt5

attached Yocto Guide and use

L3.14.28_1.0.0_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX

6Solo Linux Binary Demo Files and Linux BSP Documentation

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos