Not able to hear (using audio port) or speak (using mic port) on imx6qp SabreSD board when a call connection is established

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to hear (using audio port) or speak (using mic port) on imx6qp SabreSD board when a call connection is established

620 Views
sachinarora
Contributor I

Hi,

We are using imx6qp SabreSD eval board (with OREO 8.0) to make a call. We are able to call the other person, but Not able to hear or speak on the mic port and audio-out port.

We are able play an audio file and listen to it using the audio-out port. We are also able to record the audio using the mic port on the kit. But we are not able to hear or speak after the call connection is established.

Kindly help.

 

Regards,

 

Sachin Arora

Labels (1)
0 Kudos
1 Reply

508 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

 

Have you installed in the proper way the extended media codecs?

 

Android OS for i.MX Applications Processors | NXP 

Embedded Application Software - miscellaneous

 

For more detail on it, please, refers to the i.MX Android Extended Codec Release Note

 

Best regards,

Diego.

0 Kudos