Not able to get the source code of kk4.4.3_2.0.0.-ga

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Not able to get the source code of kk4.4.3_2.0.0.-ga

1,204 次查看
mutyalaraoneela
Contributor III

Hi all,

          I am working on IMX6 solo lite board in order to bring up android 4.4.3 on it. I am following the user guide document for downloading the source code , kernal source and uboot source.I am able to download the Kernal image and uboot image but not the source code of android. It would be great and helpful to me if any reply.

Thank you,

Mutyala Rao.

0 项奖励
回复
2 回复数

1,075 次查看
Yuri
NXP Employee
NXP Employee

   Have You tried instructions of section 3.1 [Getting Android source code (Android/kernel/U-Boot)]

of "Android_User's_Guide.pdf"  ?

http://www.freescale.com/webapp/Download?colCode=IMX6_KK443_200_ANDROID_DOCS&Parent_nodeId=133769948...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,075 次查看
mutyalaraoneela
Contributor III

Hi ,

       I followed user guide,but iam not able to patch.It is showing like

     root@cpu347:~/myandroid# c_patch /opt/android_KK4.4.3_2.0.0-ga_core_source/code/KK4.4.3_2.0.0-ga imx_KK4.4.3_2.0.0-ga
     Error! Can't read base file - /opt/android_KK4.4.3_2.0.0-ga_core_source/code/KK4.4.3_2.0.0-ga/baseversion

     please help me.

Thank you,

Mutyala Rao

0 项奖励
回复