Not able to configure IPU for 16-bit camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to configure IPU for 16-bit camera

1,015 Views
paritoshsingh
Contributor I

Hi,

I have custom camera connected to IMX6 dual lite processor through LVDS deserializer (THC63LVD1024).

LVDS deserializer (THC63LVD1024) is running in dual-in single out mode.

I have tried different configuration gathered from different threads available on freescale community but none of them worked out for me.

below are settings for getting 16 bit generic data:

IPU_CSI0_SENS_CONF register ==> 0x0400CB00

below are setting for UYVY:

IPU_CSI0_SENS_CONF register ==> 0x0400CA00

Please provide setting to configure 16-bit camera for UYVY format.

If there is some patch available than kindly let me know.

Regards,

Paritosh Singh

0 Kudos
Reply
1 Reply

856 Views
joanxie
NXP TechSupport
NXP TechSupport

How to Support RGB565 Gated Mode Input to i.MX6 CSI

this thread is for rgb565 gate mode, hope helpful for you.

0 Kudos
Reply