Not able to browse internet in YOCTO project using WiFi Dongle D-LINK DWA125

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to browse internet in YOCTO project using WiFi Dongle D-LINK DWA125

1,783件の閲覧回数
senthilkumar_s1
Contributor II

Hello All,

I am tying to ping google.com from Weston terminal in YOCTO Linux distribution.

I am able to scan and connect to the WiFi Network using WiFi Dongle D-LINK DWA125.

Not able to ping google.com. It says "bad address".

But, same i am able to ping google.com through Ethernet interface

Followed below procedure

>ifconfig wlan0 up

>iwconfig wlan0 essid "WiFi Network Name"

Note : WiFi network does not have password. So i didn't key.

>ping google.com

ping: bad address 'google.com'

Thanks,

Senthil.

ラベル(3)
0 件の賞賛
返信
1 返信

1,505件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Senthil

one can try suggestions provided on

yocto wi-fi with wl12xx | NXP Community

and post on digi community

D-Link Forums - Index

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信