Nonstandard Bit Mapping of LVDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Nonstandard Bit Mapping of LVDS

2,255件の閲覧回数
andreylipov
Contributor II

Hello, i have IMX6Q board sabreSD or sabelite.

Trying to connect it to my LVDS monitor, but my monitor have non standart LVDS, not similar to SPWG/PSWG/VESA and JEIDA standarts.

How and where i can change outputs of the LVDS bit mapping?

Using Android 4.3

Thank's for any help,

Andrey

0 件の賞賛
返信
1 返信

1,289件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andrey

LDB module can not change mapping, however

one can try to change input data using sect.37.4.7.5.1

Bus Mapping Unit IMX6DQRM - these data are used as IPU

output and LDB input, also please check Figure 19-1. i.MX53 LVDS Display

Bridge (LDB) Block MX53UG (this valid for i.MX6 too).

Best regards

igor

0 件の賞賛
返信