No vivante drivers in X11

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No vivante drivers in X11

Jump to solution
913 Views
olegpereverzev
Contributor I

Hello. I am trying to make Compulab's debian distro be more adequate for my needs, and as there no way to use Yocto for cm-fx6, i try to make everything on my own.

The problem is, that i've installed vivante drivers, and they gave me libEGL, libGL, and etc., but there is no driver for X11, that should be in /usr/lib/xorg/modules/drivers/

Where do i find it? Here is my xorg.conf: [Xorg Config] Section "Module" Load "extmod - Pastebin.com

Labels (4)
Tags (2)
0 Kudos
1 Solution
511 Views
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

you can check below for available vivante drivers

L3.10.17_1.0.0_LINUX_DOCS

L3.0.35_4.1.0_LINUX_DOCS

L3.10.17_1.0.0_IMX6QDLS_BUNDLE : Source Code

L3.0.35_4.1.0_ER_SOURCE_BSP :

If you will not find necessary drivers please post

this to meta-fsl-arm mailing list, so that someone familiar with this board

s/w distribution could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor
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
512 Views
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

you can check below for available vivante drivers

L3.10.17_1.0.0_LINUX_DOCS

L3.0.35_4.1.0_LINUX_DOCS

L3.10.17_1.0.0_IMX6QDLS_BUNDLE : Source Code

L3.0.35_4.1.0_ER_SOURCE_BSP :

If you will not find necessary drivers please post

this to meta-fsl-arm mailing list, so that someone familiar with this board

s/w distribution could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos