No private recovery resources for TARGET_DEVICE sabreauto_6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No private recovery resources for TARGET_DEVICE sabreauto_6q

5,722 Views
sunil_kumar
Contributor I

Iam using IMX.6q,iam trying to build android 5 image for my IMX.6q board,i followed Android_User's_Guide.pdf(freescale),,,,,,while compiling it is showing following error,please help me to solve this........

including ./system/media/camera/tests/Android.mk ...

including ./system/netd/client/Android.mk ...

including ./system/netd/server/Android.mk ...

including ./system/security/keystore-engine/Android.mk ...

including ./system/security/keystore/Android.mk ...

including ./system/security/softkeymaster/Android.mk ...

including ./system/vold/Android.mk ...

including ./tools/external/fat32lib/Android.mk ...

No private recovery resources for TARGET_DEVICE sabreauto_6q

make -C kernel_imx -j4 uImage ARCH=arm CROSS_COMPILE=`pwd`/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi- LOADADDR=0x10008000

make[1]: Entering directory `/home/sunil/myandroid/kernel_imx'

  CHK     include/generated/uapi/linux/version.h

  CC      scripts/mod/empty.o

arm-eabi-gcc: error trying to exec 'cc1': execvp: No such file or directory

make[3]: *** [scripts/mod/empty.o] Error 1

make[3]: *** Waiting for unfinished jobs....

  CC      scripts/mod/devicetable-offsets.s

arm-eabi-gcc: error trying to exec 'cc1': execvp: No such file or directory

make[3]: *** [scripts/mod/devicetable-offsets.s] Error 1

make[2]: *** [scripts/mod] Error 2

make[1]: *** [scripts] Error 2

make[1]: *** Waiting for unfinished jobs....

make[1]: Leaving directory `/home/sunil/myandroid/kernel_imx'

make: *** [out/target/product/sabreauto_6q/kernel] Error 2

#### make failed to build some targets (37 seconds) ####

Labels (2)
0 Kudos
Reply
2 Replies

1,280 Views
gary_bisson
Senior Contributor III

Hi,

The recovery resources is not an error but merely a warning that says that you don't have a "recovery/res" folder inside you board device folder:

Cross Reference: /build/core/Makefile

As jimmychan​ said, your error is the cc1 missing command. Please make sure to install all the required packages before building as explained in the release documentation.

Regards,

Gary

0 Kudos
Reply

1,280 Views
jimmychan
NXP TechSupport
NXP TechSupport

seems the error is "error trying to exec 'cc1': execvp: No such file or directory"

0 Kudos
Reply