No output of 'less' or 'screen' on imx28evk with 3.14 kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No output of 'less' or 'screen' on imx28evk with 3.14 kernel

1,254 次查看
CraigMcQueen
Contributor III

I'm testing the 3.14.19 kernel on imx28evk, with a Yocto build that uses the linux-fslc kernel provider. I've added the following to my local.conf to build extra packages:

 

IMAGE_INSTALL_append = " lrzsz alsa-utils screen nano strace dropbear"

 

I've found that running Busybox 'less' and GNU 'screen' both generate no output, but seem to lock up. E.g. for 'less':

 

# less /etc/passwd

 

Nothing. Ctrl-C to quit. But ordinary 'cat' works fine:

 

# cat /etc/passwd root::0:0:root:/home/root:/bin/sh daemon:*:1:1:daemon:/usr/sbin:/bin/sh ... 

 

Busybox less can be terminated with Ctrl-C. GNU screen can't be terminated with Ctrl-C, but can be terminated with Ctrl-\.

 

Running strace on 'less /etc/passwd', I see the last few lines are:

 

# strace less /etc/passwd ... fstat64(1, {st_mode=S_IFCHR|0600, st_rdev=makedev(204, 64), ...}) = 0 readlink("/proc/self/fd/1", "/dev/ttyAMA0", 126) = 12 stat64("/dev/ttyAMA0", {st_mode=S_IFCHR|0600, st_rdev=makedev(204, 64), ...}) = 0 open("/dev/ttyAMA0", O_RDONLY|O_LARGEFILE

 

It halts at that point until Ctrl-C is pressed.

 

For GNU 'screen', it's not so obvious how to make sense of it. I will attach strace output for each.

 

Any suggestions on diagnosis of this would be appreciated.

Original Attachment has been moved to: screen-strace.txt.zip

Original Attachment has been moved to: less-strace.txt.zip

标签 (2)
0 项奖励
回复
2 回复数

1,041 次查看
CraigMcQueen
Contributor III

I've reported this to the meta-freescale mailing list, and others have confirmed it and said that Busybox getty should be patched or have some extra command-line option provided. I found that this issue is resolved by modifying the getty line in /etc/intttab to add the -L option:

AMA0:12345:respawn:/sbin/getty -L 115200 ttyAMA0

It will be patched soon in the OE-core repository by the looks of it.

0 项奖励
回复

1,041 次查看
CraigMcQueen
Contributor III

I made some progress by comparing to a system running 3.14 kernel built with a different build system, which didn't exhibit the problem. If I run this command on the imx28evk:

stty clocal

then less and screen both work fine! Now I just need to understand why, and how clocal may be set on ttyAMA0 at boot time...

0 项奖励
回复