I use u-boot 2016.03 and ubuntu Image(kernel 3.14.52), I want to use LVDS as default video output, I set the u-boot variable setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb0:dev=ldb, LDB-XGA,1024x768M@60,if=RGB666'. The LVDS panel backlight flick several times then stoped. The video is always output from HDMI. Could you tell me how to set the LVDS as default output?
Below is my environment parameters:
Hit any key to stop autoboot: 0
=> printenv
active_partition=1
baudrate=115200
board=sabrelite
bootargs=cpu= board=
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,ldb=sin1,1024x768M@60,if=RGB666
bootcmd=script=/6x_bootscript;run runscript;setenv stdout serial,vga; echo ; echo 6x_bootscript not found ; echo ; echo serial console at 115200, 8N1 ; echo ; echo detai;
bootdelay=3
bootdevs=sata mmc usb
clearenv=if sf probe || sf probe ; then sf erase 0xc0000 0x2000 && echo restored environment to factory default ; fi
cmd_hdmi=fdt set fb_hdmi status okay;fdt set fb_hdmi mode_str 1280x720M@60;
cmd_lcd=fdt set fb_lcd status disabled
cmd_lvds=fdt set fb_lvds status okay;fdt set fb_lvds mode_str hannstart7;
console=ttymxc1
cpu=6Q
dfu_alt_info=u-boot raw 0x0 0xc0000
eth1addr=00:19:b8:00:00:02
ethact=FEC
ethprime=FEC
fb_lvds=hannstart7
fb_lvds2=hannstar
fdt_addr=13000000
fdt_high=0xffffffff
fileaddr=10008000
filesize=1155
initrd_high=0xffffffff
loadaddr=0x12000000
loadsplash=if sf probe ; then sf read ${splashimage} ${splashflash} ${splashsize} ; fi
mmc_disks=0 1
mmc_ums_disks=0 1
net_upgradeu=dhcp 10008000 net_upgradeu && source 10008000
otg_upgradeu=run usbnetwork; tftp 10008000 net_upgradeu && source 10008000
reset_cause=1
rundfu=dfu 0 sf 0:0:25000000:0
runscript=for dtype in ${bootdevs}; do if itest.s usb == ${dtype} ; then usb start ;fi; disks=${mmc_disks};if itest.s mmc != ${dtype} ; then disks=0;fi; for disk in ${di;
sfname=SST25VF016B
splashflash=c2000
stdin=serial,usbkbd
stdout=serial,vga
uboot_defconfig=nitrogen6q
umsdevs=sata mmc
upgradeu=script=/6x_upgrade; run runscript
usbnet_devaddr=00:19:b8:00:00:02
usbnet_hostaddr=00:19:b8:00:00:01
usbnetwork=setenv ethact usb_ether; setenv ipaddr 10.0.0.2; setenv netmask 255.255.255.0; setenv serverip 10.0.0.1;
usbrecover=run usbnetwork;setenv bootargs console=${console},115200; tftpboot 10800000 10.0.0.1:uImage-${board}-recovery && tftpboot 12800000 10.0.0.1:uramdisk-${board}-0
Environment size: 2673/8188 bytes
解決済! 解決策の投稿を見る。
Below is my solution:
env default -f -a
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,1024x768M@60,if=RGB666'
setenv fb_lvds hannstar //Because my LVDS panel's solution is 1024x768
saveenv
reset
After doing above steps, the LVDS only shows "U-boot 2016.03......" , then I power off the board and power on it several seconds. The LVDS panle is on.
Below is my solution:
env default -f -a
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,1024x768M@60,if=RGB666'
setenv fb_lvds hannstar //Because my LVDS panel's solution is 1024x768
saveenv
reset
After doing above steps, the LVDS only shows "U-boot 2016.03......" , then I power off the board and power on it several seconds. The LVDS panle is on.
Hi,
I think you can try following setting:
setenv bootargs_mmc setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb0:dev=ldb,bpp=32
And also since you mentioned "The video is always output from HDMI", so I think you may remove HDMI connection first to test it. If you want LVDS and HDMI dual display, you can try this setting:
setenv bootargs_mmc setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb0:dev=ldb video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24
Detail info you can refer to i.MX_Linux_User's_Guide.pdf, chapter 4.7.
Best regards,
Danwei Luo
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Everytime the board reset, the log from serial console is like this:
U-Boot 2016.03-20415-ged95621 (Jul 07 2016 - 17:28:42 -0700), Build: jenkins-uboot_v2016.03-64
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: POR
Board: SABRE Lite
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB
Display: lvds:hannstar (1024x768)
In: serial
Out: serial
Err: serial
Net: Micrel ksz9021 at 6
FEC [PRIME]
Error: FEC address not set.
, usb_ether
Hit any key to stop autoboot: 0
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: ncq stag pm led clo only pmp pio slum part
No port device detected!
** Bad device size - sata 0 **
MMC: no card present
MMC: no card present
** Bad device mmc 0 **
switch to partitions #0, OK
mmc1 is current device
4437 bytes read in 30 ms (143.6 KiB/s)
## Executing script at 10008000
** File not found uEnv.txt **
42869 bytes read in 1209 ms (34.2 KiB/s)
only CEA modes allowed on HDMI port
----------- trying to load /initrd.img
2317536 bytes read in 279 ms (7.9 MiB/s)
5499904 bytes read in 501 ms (10.5 MiB/s)
Kernel image @ 0x10800000 [ 0x000000 - 0x53ec00 ]
## Flattened Device Tree blob at 13000000
Booting using the fdt blob at 0x13000000
reserving fdt memory region: addr=13000000 size=b000
Using Device Tree in place at 13000000, end 1300dfff
Starting kernel ...
fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
snvs_rtc 20cc034.snvs-rtc-lp: can't get snvs-rtc clock
fsl-hdmi-dai hdmi_audio.3: failed to probe. Load HDMI-video first.
imx-audio-hdmi sound-hdmi.19: initialize HDMI-audio failed. load HDMI-video first!
imx6q-pcie 1ffc000.pcie: phy link never came up
imx6q-pcie 1ffc000.pcie: Failed to bring link up!
imx6q-pcie 1ffc000.pcie: failed to initialize host
Hi,
Thanks for your reply.
I removed the HDMI and found the LVDS shows "u-boot 2016.03 ....", I checked the serial port, it hangs on below message,
the board will reset serial times then hang on below message. But I remove LVDS and insert the HDMI, it will boot to ubuntu normally.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: ncq stag pm led clo only pmp pio slum part
No port device detected!
** Bad device size - sata 0 **
MMC: no card present
MMC: no card present
** Bad device mmc 0 **
switch to partitions #0, OK
mmc1 is current device
4437 bytes read in 30 ms (143.6 KiB/s)
## Executing script at 10008000
** File not found uEnv.txt **
42869 bytes read in 1209 ms (34.2 KiB/s)
only CEA modes allowed on HDMI port
----------- trying to load /initrd.img
2317536 bytes read in 280 ms (7.9 MiB/s)
5499904 bytes read in 501 ms (10.5 MiB/s)
Kernel image @ 0x10800000 [ 0x000000 - 0x53ec00 ]
## Flattened Device Tree blob at 13000000
Booting using the fdt blob at 0x13000000
reserving fdt memory region: addr=13000000 size=b000
Using Device Tree in place at 13000000, end 1300dfff
Hi
please look at below link describing BD ubuntu usage
https://boundarydevices.com/mx-linux-kernel-3-14-52/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
I saw the link but it doesn't resolve my issue. I tried set the LVDS parameters as below, but no effect at all.
Hit any key to stop autoboot: 0
=> setenv fb_lvds hannstar7
=> saveenv
=> reset