Dear all
I made sure that 10 inches lcd (HSD100PXN1) that work well against the Touch from i.mx6q cpu board.
So when you connect the 7 inches LVDS LMS700JF01-001 not touch the image is well Scary . The touch IC, MAX11801.
When the touch panel interrupt and I2C operation are good . However, this operation is not on the screen. The MAX11801 logo message appears that connection . Of course, X +, X-, Y +, Y- been brought up signal is properly connected.
Please comment why the touch no operation .
Hi kim
for touch test one can try ts_test (tslib package in ltib)
https://community.freescale.com/thread/317078
also it makes sense on other examples:
imx6 sabre-sdb and LCD touchscreen MAX11801
Touchscreen support on IMX6 Evaluation Kit
Configuring i.MX6 boards for different screens
http://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------