No clock ouput for mipi_dsi1_ts_scl pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No clock ouput for mipi_dsi1_ts_scl pin

861 Views
cloudfu
Contributor I

Hi there, 

I added a new i2c device(max_serdeser1) to i2c0_mipi_dsi1 bus, the driver probe could be ok but regmap_i2c_read repord err with errno '-5' as below during i2c device reg configuration procedure.  I also measured the mipi_dsi1_ts_scl pin via oscilloscope but no clk signal ouput.  Anyone can help to support.  thanks very much.

1.png2.png

log:

[ 20.237438] cloud debug max967xx_bridge_attach +++
[ 20.242236] child node panel /i2c@57226000/max967xx@40/panel@0
[ 20.249250] panel-simple panle0: panle0 supply power not found, using dummy regulator
[ 20.257202] cloud debug max967xx_bridge_attach 1
[ 20.261829] cloud debug max967xx_bridge_attach 2
[ 20.266559] nwl-mipi-dsi 57228000.mipi_dsi_bridge: lanes=4, format=0x0 flags=0x11
[ 20.274054] nwl-mipi-dsi 57228000.mipi_dsi_bridge: Bridge attached
[ 20.280246] cloud debug max967xx_bridge_attach ---
[ 20.285058] nwl-mipi-dsi 57228000.mipi_dsi_bridge: drm_bridge_attach: ret: 0
[ 20.292130] imx-drm display-subsystem: bound mipi_dsi@57228000 (ops imx_nwl_dsi_component_ops)
[ 20.374376] max967xx 3-0040: regmap_readable:ffff000008796ac4, 6915, (null), (null), ffff00000874f0e0, (null)
[ 20.374381] max967xx 3-0040: regmap_readable okay bus: ffff000009d922d0
[ 20.374512] max967xx 3-0040: map->reg_read: -5
[ 20.374644] max967xx 3-0040: DSI format is: 0

0 Kudos
6 Replies

849 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fu

 

what bsp used in the case. Recommended to try latest Linux 5.10.9_1.0.0

and build all image from scratch following Release Notes requirements for versions

of software components (like SCFW 1.8.0, e.t.c.)  i.MX Linux Release Notes

 

Best regards
igor

0 Kudos

772 Views
cloudfu
Contributor I

hello, 

how can i download the related kernel repo ? 

seems there is not tag found as below cmd:

"git clone https://source.codeaurora.org/external/imx/linux-imx -b rel_imx_5.10.9_1.0.0"

 

SCR-5.10.9_1.0.0.txt: 

NXP Software Content Register

Release - Linux 5.10.9_1.0.0
March 2021

Yocto Project recipe manifest:
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-gatesgarth -m imx_5.10.9_1.0.0.xml

Release tag: rel_imx_5.10.9_1.0.0

--------------------------------------------
BSP Packages
--------------------------------------------

Package: linux-imx.git
Outgoing License: GPL-2.0
License File: COPYING
Package Category: BSP
Type of Content: source
Description and comments: The Linux kernel with i.MX-specific drivers
Release Location: https://source.codeaurora.org/external/imx/linux-imx -b rel_imx_5.10.9_1.0.0
Origin: NXP (GPL-2.0)
kernel.org (GPL-2.0) - https://www.kernel.org/

0 Kudos

751 Views
igorpadykov
NXP Employee
NXP Employee

for Android Auto support one can look at below link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

"This software is offered through NXP Professional Services."

 

Best regards
igor

0 Kudos

840 Views
cloudfu
Contributor I

Hello, 

out change is based on imx-p9.0.0_2.1.0-auto-ga verion.  is there any issue with DSI i2c bus ? 

so your suggestion is to upgrade kernel version to 5.10.9_1.0.0 ?

 

thanks

Br

cloud fu

0 Kudos

810 Views
cloudfu
Contributor I

Hello , 

how can I fetch the kernel code(5.10.9_1.0.0)  for android release?

thanks

0 Kudos

860 Views
cloudfu
Contributor I

I will very appreciate for anyone could give a soon reply.  thanks a lot.

0 Kudos