No Spi clk in imx6ull

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No Spi clk in imx6ull

874 Views
sheraz_ali
Contributor II

Clock is not coming 

My Pin mux settings are as follows

&ecspi2 {
fsl,spi-num-chipselects = <1>;
cs-gpios = <&gpio4 22 0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_spi>;

status = "okay";
spidev@0x00 {
compatible = "spidev";
spi-max-frequency = <20000000>;
reg = <0>;
};
};

&iomuxc {
.....

pinctrl_spi: spigrp{
fsl,pins = <
MX6UL_PAD_CSI_DATA00__ECSPI2_SCLK 0x100b1
MX6UL_PAD_CSI_DATA02__ECSPI2_MOSI 0x100b1
MX6UL_PAD_CSI_DATA03__ECSPI2_MISO 0x100b1
MX6UL_PAD_CSI_DATA01__GPIO4_IO22 0x80000000
>;
};

...

No clock signal. SS0 is always high

/dev/spidev1.0 is getting enumerated

cs-gpio is coming as spi_imx  

# cat /sys/kernel/debug/gpio
GPIOs 0-31, platform/209c000.gpio, 209c000.gpio:
gpio-9 (VSD_3V3 ) out lo
gpio-19 (cd ) in lo

GPIOs 32-63, platform/20a0000.gpio, 20a0000.gpio:

GPIOs 64-95, platform/20a4000.gpio, 20a4000.gpio:

GPIOs 96-127, platform/20a8000.gpio, 20a8000.gpio:
gpio-118 (spi_imx ) out lo

GPIOs 128-159, platform/20ac000.gpio, 20ac000.gpio:
gpio-129 (flexcan-trx-en ) out lo

Let me know what am missing

Linux Kernel Version 4.15

Labels (3)
Tags (2)
0 Kudos
Reply
2 Replies

778 Views
jamesbone
NXP TechSupport
NXP TechSupport

Can you please share which BSP version are you using?
Which Board are you testing? Is the EVK board ? wihch Rev of the Board.?

Can you give more details if you are using SPIDEV to reproduced the issue?

0 Kudos
Reply

778 Views
sheraz_ali
Contributor II

I am using krogth Yocto BSP, I am using imx6ull evk, I have enabled CONFIG_SPI_SPIDEV=y in kernel

0 Kudos
Reply