No Qt platform plugin in iMX6 Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No Qt platform plugin in iMX6 Yocto

2,881 Views
gaylordlebrun
Contributor II

Bonjours to all,

I have crosscompile a Qt5 application on an PC ubuntu with Qt5 toolchain in QtCreator but when I want to execute him on the target (iMX6Q YOCTO), it shows:

This application failed to start because it could not find or load the Qt platform plugin "xcb".

Reinstalling the application may fix this problem.

Thank you in advance for quite answer

Gaylord

Tags (3)
0 Kudos
Reply
1 Reply

2,031 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Gaylord,

There are a couple of comments asking of a similar issue on the following community document: https://community.nxp.com/docs/DOC-328543

Although it looks like there are no platform plugins available so I would also recommend looking at the plugins path setting.

I hope this helps!

Regards,

0 Kudos
Reply